Using Kollmorgen Visualization Builder

To work with Kollmorgen Visualization Builder:

  1. Tag the PLCClosed Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. variables to export and map with the HMIClosed Human-Machine Interfaces - Also known as computer-human interfaces (CHI). Formerly known as man-machine interfaces. HMIs are usually employed to communicate with PLCs and other computers. Example: Entering and monitoring temperatures or pressures for further automated control or emergency response. (see Map Variables to HMI for more information).
  2. Compile your project to generate the ModbusClosed Modbus® is a serial communications protocol. it is the most commonly available means of connecting industrial electronic devices. Modbus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the Modbus protocol exist for serial port and Ethernet. It is widely used with TCP/IP over Ethernet. mapping file.
  3. Create a KVBClosed Kollmorgen Visual Builder for HMI project 1 in the KAS-IDEClosed Kollmorgen Automation Suite - Integrated Development Environment and open it.
  4. Design the HMI Panel with KVB .
  5. Save and close KVB.
  6. Save your KAS project.

  • Be aware that as soon as you change the PLC variables exported for the HMI, the mapping file must be re-imported in Kollmorgen Visualization Builder to have an up-to-date version.

Related Documents

For further information on Kollmorgen Visualization Builder, see this documentation:

KVB Manuals

Description

Kollmorgen Visualization Builder™ Quick Start Guide

The Quick Start covers these important points to:

  • Install and use Kollmorgen Visualization Builder.
  • Configure HMI Panels and PCClosed Personal Computer operated control applications.

Kollmorgen Visualization Builder™ User Manual

Contains all the content to help with Kollmorgen Visualization Builder.

Concept Link IconSee Also